48049-137-05EN

Communication Module Setup

Use “Com. setup” menu to set communication module setup.

NOTE: Com. setup parameters can only be entered if a circuit breaker communication module (BCM) is installed.

Communication Module Setup

1.

Set communication parameters. Default values are:

Address = 47

Baud-rate = 19.2k

Parity = even

Set Modbus Com Values

WARNING
Potential compromise of system availability, integrity, and confidentiality
Change default passwords at first use to help prevent unauthorized access to device settings, controls and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
2.

Remote access.

Remote access is factory set and does not require adjustment.

NOTE: Remote access setting can be changed to allow protection settings to be changed via the communication network. Contact the local sales office about the availability of software to utilize this feature.

Check Remote Access

3.

Set remote control.

Manual: The circuit breaker cannot be opened or closed via the network system management software.

Auto: The circuit breaker can be opened or closed via the network system management software.

NOTE: For remote operation of the circuit breaker, the BCM must be set to enable opening and/or closing and circuit breaker must have communicating shunt coils with wire harness installed.

Set Remote Control

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.