48049-137-05EN

Phase Rotation Protection

Protects the circuit when two of the three phases are reversed.

  • If one of the phases is down, this protection is inactive.

  • Options are ABC or ACB.

  • When system frequency is set to 400 Hz, phase rotation protection is disabled.

  • Do not use phase rotation protection to determine the loss of multiple phases in delta connected systems.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.