48049-137-05EN

Contact Wear

This displays the amount of contact wear on the contact with the greatest wear. When this number reaches 100, it is recommended that a visual inspection of the contacts be done. This function works only on MasterPact® NT and NW circuit breakers.

Check Contact Wear

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.