48049-137-05EN

Graphic Display Screen

Graphic Display Screen

The graphic display screen (A) shows the trip unit settings and information. Navigation buttons (B) are used to display and modify items on the screen. Default display shows current levels.

Trip unit must be powered for graphic display screen to operate. The trip unit is powered if:

  • circuit breaker is on and has more than 150 V of load voltage on two phases (circuit breaker is closed or bottom fed).

  • the full-function or hand-held test kit is connected and on.

  • the 24 Vdc external power supply is connected.

  • an external voltage tap is installed and voltage of more than 150 V is present on two phases.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.