48049-137-05EN

Maintenance Menu

Use the maintenance button to access the maintenance menu.

A To access the history log
B To set up the M2C/M6C contacts
C To set up the MicroLogic trip unit
D To set up the metering parameters
E To set up the communication module

Maintenance Menu

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.