48049-137-05EN

Current Levels

Ia Instantaneous A phase current

Maximum measurements can also be reset to zero.

Check Current Levels

Ib Instantaneous B phase current
Ic Instantaneous C phase current

In

Instantaneous neutral current
Instantaneous ground current

Iamax

Maximum instantaneous A phase current
Ibmax Maximum instantaneous B phase current
Icmax Maximum instantaneous C phase current
Inmax Maximum instantaneous neutral current
Maximum instantaneous ground current
Voltage is above set maximum
Demand B phase current

Demand C phase current

Demand neutral current
Maximum demand A phase current
Maximum demand B phase current
Maximum demand C phase current
Maximum demand neutral current
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.