48049-137-05EN

Power Levels

P Instantaneous active power
NOTE: To ensure reliable power and power factor measurements, Set Power Sign, and Set Sign Convention.

Check Power Levels

Q Instantaneous reactive power
S Instantaneous apparent power
Power Factor Instantaneous power factor
Demand active power
Demand reactive power
Demand apparent power
Maximum demand active power
Maximum demand reactive power
Maximum demand apparent power
Maximum measurements can also
be reset to zero.
   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.