DOCA0270EN-03

Analog I/O Module Specifications

Input / Output Specifications

Channel

Inputs

Output

Rated power supply

24 Vdc

Resolution, maximum

16 bits, or 15 bits + sign

12 bits (4096 points)

Cable length, maximum

30 m (98 ft) shielded cable

Signal Type: Inputs

Channel

Inputs

Signal type

Voltage

Current

Thermocouple

3–wire RTD

Range

0–10 Vdc
−10 to +10 Vdc

0–20 mA
4–20 mA

Type K, J, R, S, B, E, T, N, C

PT100, PT1000, NI100, NI1000

Signal Type: Output

Channel

Output

Signal type

Voltage

Current

Range

0–10 Vdc
−10 to +10 Vdc

0–20 mA
4–20 mA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?