DOCA0270EN-03

Required Tools

The following table lists the tools required for installing the TeSys island.

Required tools

Tool Size
Torque driver 6 mm flat head
Torque driver #2 Phillips
Torque hex key 4 mm hexagonal

In addition, you need the following documentation:

  • Bill of materials (BOM)

  • Island topology: the order in which the TeSys island modules must be installed on the TeSys island

Verify that the modules you received match the BOM and the TeSys island topology before starting the installation. TeSys island modules must be installed in a specific order on the island. If the physical arrangement of the modules on the TeSys island does not match the configured topology, the TeSys island will not function properly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?