DOCA0270EN-03

Device Events

If device events are present on the island:

  • A red alert symbol appears in Island view above the devices that have experienced an event

  • The LEDs on the physical devices flash red

Device Event

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?