DOCA0270EN-03

Units

To change the units of measurement displayed in the OMT, perform the following steps:

  1. In the USER PREFERENCES window, click UNITS.

  2. Change the settings as desired. For more information about the settings, refer the following table.

    OMT settings for units of measurement

    Unit

    Options

    Impacts

    Motor Power

    kW, hp

    • Instantaneous Total Active Power

    • Maximum Total Active Power

    Temperature

    °C, °F

    • Motor Overheat chart - Trip Status

    • Motor Overheat options - Thermal Protection settings

    Date

    dd/mm/yyyy, mm/dd/yyyy

    • Banner time display

    • Log displays

    • Trip registers

    • Timestamp values for energy, power and voltage monitoring

  3. Click Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?