DOCA0270EN-03

Connecting Your Tablet and Using the OMT

The section explains how to connect your tablet to the TeSys island bus coupler. To perform this procedure, the island must be on the network and able to communicate with the tablet using a wireless or wired connection.

Once connection to the bus coupler is established, you can access the OMT.

Perform the following steps to connect the tablet to the OMT:

  1. Enter the address (format: https://xxx.xxx.xxx.xxx) of the bus coupler into the web browser on your tablet to access the OMT running on the bus coupler.

    NOTE: The recommended browsers are Chrome or Safari.
  2. If you are taken to the page, "Your Connection is not private":

    1. Click the Advanced button.

    2. Click the link Proceed to xxx.xxx.xxx.xxx (unsafe) to continue.

      Result: The OMT login screen is displayed on the screen.

      OMT Login Screen

  3. When connecting for the first time, enter admin as the username and schneider18 as the password.

  4. Click Login.

    Result: You will be prompted to change your password.

  5. Enter schneider18 as the current password.

  6. Enter your new password twice and click Submit.

    NOTE: Passwords must contain a minimum of 10 characters, with at least one alphabetic and one numeric character.

    Change Password

Once you log in, the CONTROL PANEL window is displayed in the OMT home screen. If you do not have permission to access the CONTROL PANEL, the Avatar View window is displayed in the OMT screen. The name of the connected TeSys island is displayed at the top of the status banner. Also displayed are the date and time, and the type of control that has been granted. See Type of Control.

Type of Control

FULL-CONTROL

This type of access is granted to the first user that logs in to the TeSys island. This user has full control of the system.

READ-ONLY

This type of access is granted to any additional users that log in to the system while another user is connected with FULL-CONTROL access. These additional users are granted read-only access, since only one user can have full control at a time.

The following information is displayed on the OMT Home Screen:

  • The number of critical and non-critical alarms.

  • An indicator flashes red when Test Mode or Force Mode is active.

  • The Hello message, confirming that you are currently logged in to the system.

  • The option to Logout of the OMT.

  • A question mark (?) you can click to get help.

OMT Home Screen

The OMT home screen provides access to a variety of task-oriented panels. Select the desired panel by clicking the corresponding button on the left side of the screen:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?