SIL Interface Module Wiring
Using the TeSys island topology and bill of materials, determine the location of the SIL* interface modules (SIMs) on the TeSys island. The SIM is supplied 24 V power and also connects to an external SIL rated device using a spring terminal connector provided with the SIM. Use the following guidelines to complete the 24 V power wiring between the SIL interface modules and the external SIL rated device.
SIM Terminal Block Pinout
|
Pin Number |
Terminal Identification |
Signal |
|---|---|---|
|
1 |
13 |
MIRROR IN |
|
2 |
K1 |
SIL-IN 1 |
|
3 |
KC |
SIL COMMON |
|
4 |
K2 |
SIL-IN 2 |
|
5 |
14 |
MIRROR OUT |
-
Remove the spring terminal connector. It is positioned on the top of the module, behind the flat cable connection.
-
Using the SIM wiring table, connect 24 V to both K1 and K2 on the removable spring terminal connector, regardless of the control architecture. In wiring category 1 and 2 applications, terminals K1 and K2 must be shorted together. See Accessories Cabling for cable types and sizes.
-
Insert the spring terminal connector back into the top of the SIM.