DOCA0270EN-03

System Event Log Attributes

System Event Log attributes are defined in the following table.

Attribute

Description

timestamp

The system time

YYYY-MM-DDThh:mm:ss.mmm

Example: 2018-01-02T15:02:59.970

avatarName

The user defined avatar name

avatarNumber

The number of the avatar in the digital tool

avatarSILGroup

The SIL* group of the avatar

deviceTag

The user defined device tag

deviceNumber

The number of the device in the physical order of the system (the Node ID on the internal bus)

value

The new value of the data change event being logged.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?