DOCA0270EN-03

Derating Examples

Example 1 – Derating Required

Load rating

8 A

Derating factor: Temperature inside the enclosure is 60 °C (140 °F)

1.20

Maximum load rating of starter TPRST009

9 A

8 A * 1.20 = 9.60 A

Since 9.60 A is greater than the maximum load rating of 9 A, derating is required. Upgrade from the TPRST009 reference number to the TPRST025 reference number with a maximum load rating of 25 A.

Example 2 – Derating Not Required

Load Rating

6 A

Derating Factor: Temperature inside the enclosure is 60 °C (140 °F) + Vertical Mounting

1.2 + (1.2 x 20%) = 1.44

Maximum Load Rating of TPRST009

9 A

6 A * 1.44 = 8.64 A

Since 8.64 A is less than the maximum load rating of 9 A, derating is not required. The TPRST009 reference number is appropriate.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?