DOCA0270EN-03

Digital I/O Module Specifications

Digital I/O Module Input Specifications

Channel

Inputs

Rated power supply

24 Vdc

Input type

Type 1 (IEC/EN/UL/CSA 61131-2)

Rated input voltage

24 Vdc

Cable length, maximum

30 m (98 ft)

Digital I/O Module Output Specifications

Channel

Inputs

Rated output voltage

24 Vdc

Rated output current

0.5 A, resistive

Cable length, maximum

30 m (98 ft)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?