DOCA0270EN-03

Avatar

The following avatar settings can be viewed or modified. For more information on avatar settings, refer to the TeSys™ island DTM Online Help Guide, 8536IB1907.

General

  • Control Mode

    • Control Mode Selection

  • Combined PV Control
    (see Configuration below)

  • FLA

Configuration

  • PV Inputs

    • PV Input Control Source

    • PV Input Control Type

    • PV Input Control Level

    • PV Input Control Hysteresis

    • PV Input Control Logic

NOTE: The Input Source can only be accessed in the DTM.

Predictive Alarms

  • Alarm Input

    • Type of Input

    • Alarm High Threshold Value

    • Alarm Low Threshold Value

  • Alarm Definition

    • Type of Protection

    • PV Input Trigger

    • Alarm Message

 

Thermal protection

  • Thermal Overload

    • Thermal Overload Trip

    • Trip Class

    • Reset Threshold

    • Motor Auxiliary Fan Cooled

    • Thermal Overload Alarm

    • Overload Alarm Level

  • Motor Overheat

    • Motor Overheat Trip

    • Trip Delay

    • Trip Level

    • Reset Threshold

    • Motor Overheat Alarm

    • Alarm Threshold

    • Temperature Sensor

Electrical Protection

  • Current Phase Loss

    • Trip

    • Trip Delay

    • Trip Level

  • Ground Current Detection

    • Trip

    • Trip Delay

    • Trip Level

    • Alarm

    • Alarm Level

  • Current Phase Unbalance

    • Trip

    • Trip Delay - Start

    • Trip Delay - Run

    • Trip Level

    • Alarm

    • Alarm Level

  • Phase Reversal

    • Trip

Load Protection

  • Jam

    • Trip

    • Trip Delay

    • Trip Level

    • Alarm

    • Alarm Level

  • Long Start

    • Trip

    • Trip Delay

    • Trip Level

  • Stall

    • Trip

    • Trip Delay

    • Trip Level

  • Undercurrent

    • Trip

    • Trip Delay

    • Trip Level

    • Alarm

    • Alarm Level

  • Overcurrent

    • Trip

    • Trip Delay

    • Trip Level

    • Alarm

    • Alarm Level

  • Rapid Cycle Lockout

    • Lockout

    • Timeout

  • Rapid Restart Lockout

    • Lockout

    • Timeout

Automatic Reset

  • Thermal

  • Electrical

  • Load

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?