DOCA0270EN-03

Stall

The Stall function detects high current intensity, typically associated with a locked or stalled motor, while in the Start state.

If enabled, this protection function triggers a Stall trip when the motor is in the Start state, and the maximum phase current exceeds the specified Stall Trip Level for a time longer than the specified Stall Trip Delay.

NOTE: No Stall detection alarm is associated with this function.

Stall and Trip

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

A

Imax

B

Imax ≥ Stall Trip Level

C

Start State

D

Stall Trip

T

Stall Trip Delay

This function is typically enabled in addition to the Long Start protection function, setting a higher acceptable current intensity level and a shorter trip delay.

Stall Trip Versus Long Start Trip

D

Stall Trip

E

Stall Level

F

Long Start Trip Level

G

Long Start Trip Delay

I

Current

Ir

Rated Current

t

Time

T

Stall Trip Delay

NOTE: In this illustration, the Stall protection function triggers a trip—while the Long Start protection function does not (because the Long Start Trip Delay has not elapsed yet).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?