DOCA0270EN-03

Mounting the Bus Coupler on DIN Rail

To install the bus coupler on the DIN rail, position the top groove of the bus coupler on the top edge of the DIN rail and press it against the rail until you hear the clip snap into place. See the figure below.

DIN Rail Installation (mm/in.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?