DOCA0270EN-03

Power Interface Module

Power interface modules (PIMs) provide the following:

  • Electrical and thermal protection functions

  • Digital asset management

TeSys avatars that include power devices can provide full-load energy monitoring when a voltage interface module is installed on the TeSys island.

A PIM can be associated with an analog I/O module to measure temperature through an external sensor. A PIM can also control and monitor the current supplied to an external device.

The main functions of the PIMs are as follows:

  • Measure electrical downstream data related to the load

  • Provide energy monitoring data when a voltage interface module is installed on the TeSys island

The PIMs are connected:

  • Upstream to a circuit breaker

  • Downstream to an external power device like a contactor, soft starter, or variable speed drive

The PIMs communicate with the bus coupler, sending operational data and receiving commands.

Power Interface Module Ratings

Power Ratings

Amperage

Reference

kW

hp

4

5

0.18–9

TPRPM009

18.5

20

0.76–38

TPRPM038

37

40

4–80

TPRPM080

Power Interface Module Features

Flat cable (for connection with the module to the left)

QR code

LED status indicators

Name tag

Upstream power connections

Downstream power connections

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?