DOCA0270EN-03

Energy Monitoring Panel

In the Energy Monitoring panel, you can access voltage monitoring, power monitoring, and energy monitoring for the system and for each TeSys™ avatar.

Voltage monitoring is only available for the System avatar. For the avatars, Time of Use is available for the Active Energy and Reactive Energy for up to four channels.

  1. Click the Energy Monitoring panel.

  2. Select the avatar.

In this panel, you can also reset any of the monitoring counters by clicking Reset.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?