DOCA0270EN-03

Operation and Maintenance Tool

The Operation and Maintenance tool (OMT) is web-based and optimized for use with a tablet so a technician can troubleshoot and diagnose the island without opening the electrical panel. The operation and maintenance tool offers the following features to aid in operation, maintenance, and troubleshooting:

  • Customizable user interface

  • User access and rights management for secure login

  • Monitoring of device behavior, load behavior, and energy consumption

  • Test mode and Force mode available for ease of maintenance

  • Diagnostics to check the island’s status and monitor the TeSys avatars

  • Control panel to operate the island directly

  • Maintenance alarms to help avoid machine down time

  • Access to product data for asset management

  • Accessibility from the engineering tools with a QR scan

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?