DOCA0270EN-03

General Installation Guidelines

This section contains information that is helpful for planning a TeSys island system. It includes requirements for enclosing the island in protective housing and for selecting the power source.

@New in Draft1 V3
NOTICE
Equipment damage
Do not swap or add modules while the power is on.
Failure to follow these instructions can result in equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?