DOCA0270EN-03

Thermal Considerations

The following tables list maximum thermal dissipation values for planning your TeSys island cooling system. The values assume maximum bus voltage, maximum field-side voltage, and maximum load currents. Typical values are often lower.

Maximum Thermal Dissipation Values: Starters and Power Interface Modules

Module Type

Reference Number

Maximum Thermal Dissipation @ AC3
(W)

Maximum Thermal Dissipation @ AC1
(W)

Standard Starters

TPRST009

3.5

5.1

TPRST025

6.6

8.3

TPRST038

11.8

12.8

TPRST065

20.3

30.5

TPRST080

30.5

30.5

SIL* Starters

TPRSS009

3.5

5.1

TPRSS025

6.6

8.3

TPRSS038

11.8

12.8

TPRSS065

20.3

30.5

TPRSS080

30.5

30.5

Power Interface Modules

TPRPM009

0.6

1.3

TPRPM038

0.9

1.0

TPRPM080

2.3

2.3

Maximum Thermal Dissipation Values: Bus Coupler, SIL Interface Module, Voltage Interface Module, I/O Modules

Module Type

Reference Number

Maximum Thermal Dissipation
(W)

Bus Coupler

TPRBCEIP

5.00

TPRBCPFN

5.00

TPRBCPFB

5.00

SIL Interface Module

TPRSM001

1.25

Voltage Interface Module

TPRVM001

0.20

Digital I/O Module

TPRDG4X2

1.20

Analog I/O Module

TPRAN2X1

1.70

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?