DOCA0270EN-03

Reset Trips

If a protection trip occurs on your avatar, execute this command to reset all trips on the TeSys island.

Perform the following steps:

  1. Click the Control Panel icon.

  2. Click Reset Trips.

    Result: All trips on the TeSys island are reset.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?