DOCA0270EN-03

Handling the Micro SD Card

When handling the micro SD card, observe the following precautions to help prevent the corruption or loss of internal data, or the malfunction of a micro SD card.

NOTICE
Loss of Application Data
  • Backup SD card data regularly.
  • Do not remove power, reset the controller, or remove the SD card while it is being accessed.
  • Orient the SD card correctly when inserting it into the controller.
  • Use only micro SD cards formatted using FAT32.
Failure to follow these instructions can result in equipment damage.

When using TeSys island and a micro SD card, observe the following precautions to help avoid data loss.

  • Accidental data loss can occur at any time. Once data is lost it cannot be recovered. Backup the SD card data regularly.

  • If you forcibly extract the micro SD card, data on the micro SD card may become corrupt.

  • Removing a micro SD card that is being accessed could damage the micro SD card, or corrupt its data.

  • If the micro SD card is not positioned correctly when inserted into the controller, the data on the card and the bus coupler could become damaged.

  • If you are updating the TeSys island firmware, be sure to update the SD card backup also.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?