DOCA0270EN-03

Avatar Monitoring

The monitoring functions described in the following tables apply to the TeSys avatars individually.

Power Monitoring

  • Instantaneous Total Active Power (kW)

  • Maximum Total Active Power (kW) and Timestamp

  • Instantaneous Total Reactive Power (kvar)

  • Maximum Total Reactive Power (kvar) and Timestamp

  • True Power Factor

  • Minimum True Power Factor and Timestamp

  • Maximum True Power Factor and Timestamp

Energy Monitoring

  • Total Active Energy (kWh)

  • Total Reactive Energy (kvarh)

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?