DOCA0270EN-03

Adding a New User

The administrator can add a new user to the OMT.

  1. Click the green plus sign in the user Management section. The Add User window appears.

    Add User

  2. Enter the following information for the new user:

    • Complete Name

    • User Name

    • Password

  3. Select the group to be assigned to the new user from the drop-down menu.

    • Administrator

    • Automation Engineer

    • Maintenance Level 1

    • Maintenance Level 2

    • Operator

    Add User Drop-down Menu

  4. Click Submit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?