DOCA0270EN-03

Importing the Project File to the DTM

This section describes how to import the project file generated with the TeSys™ island Configurator tool into the TeSys island DTM.

NOTE: SoMove™ software and the TeSys island DTM are available as downloads from www.schneider-electric.com.

Open SoMove™ software then perform the steps in the following tables.

In the Start screen

Step

Action

1

Under Project, click create a Project OFF-line.

2

In the Select a Device screen, click TeSys island and then click Create.

In the TeSys island DTM

Step

Action

1

Click Device at the top of the screen and select Import -> Import Pre-Sales Format from the drop down menu.

2

A pop-up window will appear. Click Yes to continue.

In the Open File screen

Step

Action

1

Locate the .XML file that you want to import.

2

Click on the file that you want to import. The name of the file will now be displayed in the File Name field.

3

Click the Open button.
The island configuration has now been imported into the TeSys island DTM.

In the TeSys island DTM

Step

Action

1

Click File -> Save As and enter the name of the island in the File Name field..

2

Click the Save button.

Result: The initial .xml configuration file is now converted to a new .psx SoMove project file.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?