DOCA0270EN-03

Avatar Settings

WARNING
Unintended equipment operation
  • Be sure to set the protection function parameters according to the required protection level of the controlled motors and loads.
  • TeSys™ GV2 motor circuit breakers should not be used with TeSys island for loads with trip classes set above trip class 15.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Configure the protection functions for each TeSys™ Avatar. Protection functions vary based on the Avatar selected.

Avatar Settings

Step

Action

1

Click on the SETTINGS tab in the DTM tool.

2

Under AVATARS, click the Avatar to be configured.

3

Configure the protection functions for each Avatar.

4

Click OK to confirm the settings. Save the project.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?