DOCA0270EN-03

Load Protection

Load protection settings values

Setting Name Value Range Default Value Increment
Jam Trip Delay 1–30 s 5 s 1
Jam Trip Level 100–800% 200% 1
Jam Alarm Level 100–800% 200% 1
Undercurrent Trip Level 30–100% 50% 1
Undercurrent Trip Delay 1–200 s 1 s 1
Undercurrent Alarm Level 30–100% 70% 1
Long Start Trip Delay 1–200 s 10 s 1
Long Start Trip Level 100–800% 100% 1
Rapid Cycle Lockout Timeout 1–9999 s 300 s 1
Rapid Restart Lockout Timeout 1–9999 s 300 s 1
Overcurrent Trip Level 30–800% 200% 1
Overcurrent Trip Delay 1–250 s 10 s 1
Overcurrent Alarm Level 100–1000% 180% 1
Stall Trip Delay 1–30 s 5 s 1
Stall Trip Level 50–1000% 250% 1
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?