DOCA0270EN-03

Enabling Degraded Mode Auto-Reset

NOTE: The Auto-Reset function may lead to immediate energizing of the load, with an active command from the PLC or the Force mode function.
WARNING
UNINTENDED EQUIPMENT OPERATION
Configure the Degraded Mode Auto-Reset in such a way that it does not result in hazardous conditions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Under Fieldbus, select Logic Controller.

  2. Set Enable Degraded Mode Auto-Reset to Yes.

Enabling Degraded Mode Auto-Reset

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?