DOCA0270EN-03

Avatar View Panel

In the Avatar View panel, you can do the following:

  • Display status and counter information about a selected TeSys avatar

  • Reset Minor Events, as well as trip and alarm counters, for the avatar

This panel includes an I/O view and a Counters view.

  1. Click the Avatar View panel to display a list of avatars configured on the TeSys island.

  2. Perform avatar maintenance tasks as necessary.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?