DOCA0270EN-03

Settings Panel

The OMT can be used to view the system settings as well as individual TeSys™ avatar settings. If your OMT access level permits, you can also edit any of the system and individual avatar settings. Settings are configurable for the system, load, and device avatars to enable energy monitoring and to customize the avatar parameters.

For assistance in selecting the settings, refer to the DTM online help or the TeSys™ island DTM Online Help Guide, 8536IB1907. In the OMT tool, press F1 for help.

NOTE: TeSys GV devices should not be used with TeSys island for loads with trip classes set above trip class 15.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?