DOCA0270EN-03

Island Orientation

TeSys island can be mounted horizontally without derating. TeSys island can also be mounted vertically with 20% derating. The maximum width of the TeSys island is 112.5 cm (3.83 ft), measured from the bottom left edge of the bus coupler to the right edge of the last module on the TeSys island. See the figures below.

  • Horizontal mounting: The bus coupler (A) must be the left-most component on the TeSys island.

  • Vertical mounting: The bus coupler (A) must be the bottom-most component on the TeSys island.

Bus Coupler in Horizontal Orientation

Bus Coupler in Vertical Orientation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?