DOCA0270EN-03

Motor Two Speeds Two Directions

Two Speed Wiring

Accessories

Legend

A

Mechanical interlock

B

Parallel link

C

Reversing link

F

Forward

R

Reverse

LS

Low speed

HS

High speed

ST-1

Starter 1

ST-2

Starter 2

ST-3

Starter 3

ST-4

Starter 4

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?