DOCA0270EN-03

Connecting to TeSys™ island with SoMove™ Software

Perform the steps in the following table the first time you connect to TeSys island with a PC running SoMove software and the TeSys island DTM. SoMove software is a Microsoft® Windows®-based application using open FDT/DTM technology. SoMove contains DTMs for different devices. The TeSys island DTM enables the configuration, monitoring, control, and customization of TeSys island functions.

NOTE: Ensure that you always use the latest version of TeSys island DTM.

Connecting to the TeSys island with SoMove Software

Step Action

1

Check the LED indicators on the bus coupler and verify that power is applied. Verify that the PWR LED, indicating the power supply and system status, is steady green, and the MS LED, indicating the bus coupler status, is flashing green.

2

Connect a PC (with SoMove software and the TeSys island DTM installed) to the terminal/service port on the bus coupler using an RJ45 cable.

3

Launch the SoMove software on the PC.

4

Click the Connect button in the Start screen.

5

In the Scan Result dialog box, click the Modbus TCP tab.

6

Click the edit symbol next to the question mark.

7

In the Advanced settings dialog box, enter the network address of the TeSys island in the Target address. The network address by default is 10.10.0.1 or enter the IP address that was assigned using the OMT.

8

Select Single as the Scan Type and click OK.

9

Click Scan Network in the Scan Result dialog box.

10

Select the TeSys island device and click Connect.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?