DOCA0270EN-03

Avatar Minor Events

@New in Draft1 V03

TeSys island logs the following Avatar Minor Event events:

  • Asset Alarm

  • Device Mismatch

  • Device Data not updated

  • A mismatch between the installed modules and the modules defined in the context file

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?