DOCA0270EN-03

Counters and Minor Event Reset

To access the trip and alarm counters for the system, or to reset Minor Events, click the Counters tab in the System Avatar window. The following information is displayed in Counters view:

  • System Minor Events

  • Fieldbus Comm. Events Counter

  • System Alarms Counter

  • Minor Events Record

To reset the System Minor Events, Fieldbus Comm. Events Counter, or the System Alarms Counter, click the Reset button.

Reset Window

@Updated in Draft1 V03

To reset the Avatar Minor Event counter, click the Reset option on the respective avatar window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?