DOCA0270EN-03

Exit Force Mode

Once you complete the Force mode activities, you must manually exit Force mode to return the island to the operational state:

  1. Click the Diagnostics View panel.

  2. Click the Exit Force mode button.

    Exit Force Mode

  3. A pop-up appears. To confirm that you want to exit Force mode, click Yes.

Exit Force Mode Confirmation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?