DOCA0270EN-03

System

The following settings can be viewed and modified for the System avatar.

Fieldbus

  • IP Address

  • Subnet

  • Gateway

  • IPv6 Address

  • IP Mode

  • Network Name

  • Communication Loss Timeout

NOTE: For the definition of a communication loss, see Degraded Mode.

Fast Device Replacement (FDR)

  • FDR Enable

  • FDR Synchronization Enabled

  • FDR Synchronization Period

  • FDR Data Restore—Command

  • FDR Data Backup—Command

System

  • SD Log Update Period

  • Force Mode Data Retention

  • Test Mode Allowed

  • Force Mode Allowed

Voltage

  • Voltage Dip Threshold

  • Voltage Swell Threshold

For more information on System settings, refer to the TeSys™ island DTM Online Help Guide, 8536IB1907.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?