DOCA0270EN-03

Locate Command

In Island View, click the Locate button to physically locate the connected island. The bus coupler’s PWR LED illuminates a steady yellow for 5 s to help you identify which device the OMT is communicating with.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?