DOCA0270EN-03

Verifying the System Wiring

After all required and optional parameters have been configured and you have tested the functionality of the power devices, check the system wiring, which can include:

  • Power wiring (see the table below)

  • Bus coupler connections (see the table below)

  • I/O wiring

  • SIL* interface module wiring

  • Voltage interface module wiring

Perform the steps in the following table to verify the power wiring.

Verify the Power Wiring

Step

Action

1

Visually confirm that the actual power wiring matches the intended power wiring, as described in the power wiring diagram.

2

Look for any detected trips or notifications in the OMT or DTM.

Verify the Bus Coupler Connections

Step

Action

1

Verify that the Fieldbus connections are in place.

2

Verify that the 24 V control power connection is securely in place.

3

Verify that the flat cables from the bus coupler to all modules are securely in place

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?