DOCA0270EN-03

Rapid Restart Lockout

The Rapid Restart Lockout function helps prevent potential harm to the motor caused by repetitive, successive stop and start events.

If this protection function is enabled, the TeSys avatar ignores Run commands for the duration specified by the Rapid Restart Lockout Timeout, starting from the last transition to the motor Off state .

No alarm or trip is associated with this function.

Rapid Restart Lockout

Ir

Rated Current

I

Current

A

Rapid Restart Lockout Timeout

B

New Run Commands Ignored

C

New Run Commands Not Ignored

D

Transition to Motor Off State

t

Time

   

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?