DOCA0270EN-03

Ethernet Network Topologies

TeSys island can be used in a star or ring topology. TeSys island supports Rapid Spanning Tree Protocol (RSTP), a network protocol that builds a loop-free logical topology for Ethernet networks. RSTP is enabled by default in the system avatar.

NOTE: External managed switches need to be connected.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?