DOCA0270EN-03

Undercurrent

The Undercurrent function detects unexpected low current consumption during the Run state. This condition is typically associated with motors running free, without a load—for instance, if a drive belt or shaft has broken.

If enabled, this protection function performs the following:

  • Signals an Undercurrent Alarm when the average phase current remains below the specified Undercurrent Alarm Level

  • If the motor is in the Run state, triggers an Undercurrent Trip when the average phase current remains below the specified Undercurrent Trip Level, for a time longer than the specified Undercurrent Trip Delay

Undercurrent Trip and Alarm

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

A

Iavg

B

Iavg ≤ Undercurrent Alarm Level

C

Iavg ≤ Undercurrent Trip Level

D

Run State

E

Undercurrent Alarm

F

Undercurrent Trip

T

Undercurrent Trip Delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?