DOCA0270EN-03

I/O Module Wiring

Use the following guidelines and refer to the TeSys Avatar wiring diagrams to wire the I/O modules.

  1. Remove the spring terminal connector. It is positioned on the top of the module, behind the flat cable connection.

  2. Refer to the table and figures below and make the power and control connections. See Accessories Cabling for cable types and sizes.

  3. Insert the spring terminal connector back into the top of the module.

Digital I/O Module Terminals

Analog I/O Module Terminals

Pin Digital I/O Module Terminal Identification Analog I/O Module Terminal Identification
1
(closest to DIN rail)
Input 0 I0 Input 0 + I0+
2 Input 1 I1 Input 0 – I0–
3 Input Common IC NC 0 NC0
4 Input 2 I2 Input 1+ I1+
5 Input 3 I3 Input 1 – I1–
6 Output 0 Q0 NC 1 NC1
7 Output Common QC Output + O+
8
(closest to front face)
Output 1 Q1 Output – O–
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?