DOCA0270EN-03

Standard Starters

Standard starters provide load control, electrical and thermal protection functions, and digital asset management.

Starters provide the following main functions:

  • On/Off power control for loads (three phase or single phase)

  • Electrical data measurement related to the load

  • Energy monitoring when a voltage interface module is installed on the TeSys island

  • Functional testing and simulation

  • Event logging and counters

Multiple starters might be needed for a single TeSys avatar function. For example, a motor two-direction avatar includes two standard starters.

The standard starters are connected:

  • Upstream to a circuit breaker

  • Downstream to the load (three phase or single phase)

The starters communicate with the bus coupler, sending operational data and receiving commands.

Standard Starter Ratings

Power Ratings

Amperage

Reference

kW

hp

4

5

0.18–9

TPRST009

11

15

0.5–25

TPRST025

18.5

20

0.76–38

TPRST038

30

40

3.25–65

TPRST065

37

40

4–80

TPRST080

Standard Starter Features

Flat cable (for connection with the module to the left)

Name tag

LED status indicators

Mobile bridge

Upstream power connections

Downstream power connections

QR code

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?