BRU9950900-01

Integrated Cable Test Facility

Safety Provisions

WARNING
HAZARD OF INCORRECT OPERATION
  • Only qualified operator must perform the test and following safety regulations.
  • Do not use any tools other than specified for integrated cable test facility.
  • Do not loosen any screw, nut, element other than that provided for in this operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Cable Testing

Cable testing involves injecting a test voltage through a cable between two Ringmaster AirSeT units A and B.

Cable Testing

The main purposes of cable testing via voltage injection are:

  • Ensuring the integrity of the cable between substation before energizing it.

  • To locate a fault on a cable (or on a phase if more than 1 cable per phase).

  • To diagnose and localize potential problems on a cable.

WARNING
HAZARD OF INCORRECT OPERATION
Ensure the earth collector or one of the voltage injection fingers are not damaged, if damaged (bended, sheath damaged, or other), stop operations and contact the field service representatives.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The integrated cable test facility:

  • Helps eliminate the need to open the connection compartment to access the cable connections.

  • Provides a full interlock with the earthing switch.

  • Facilitates the cable connection with specific injection fingers.

The integrated cable test facility is located at the front of the Ringmaster AirSeT unit.

Cable Test Facility


1

Withdrawable earth collector

4

Fixed contacts

2

Injection fingers

5

Earth finger

3

Earth collector locking knob

6

Injection point

Maximum Injection Voltage for Test Signal

NOTICE
HAZARD OF ELECTRICAL BREAKDOWN
When testing the cable of the Ringmaster AirSeT, limit the voltage and duration as shown in the below Table – Voltage Test of Ringmaster AirSeT.
Failure to follow these instructions can result in equipment damage.

Voltage Test of Ringmaster AirSeT

Test Voltage

Voltage per min

DC (positive/negative)

32 kV/15 min

VLF (Very Low Frequency)

22 kV/60 min

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?