BRU9950900-01

Storage

CAUTION
HAZARD OF INAPPROPRIATE STORAGE CONDITIONS
  • Keep the device in its original packaging until its final installation.
  • Do not install the device if there are any signs of damage.
  • Comply with the storage conditions if the unit is not being installed immediately.
Failure to follow these instructions can result in injury or equipment damage.
If the unit are not installed immediately after delivery, they can be stored under the following conditions:
  • The Ringmaster AirSeT unit is suitable for indoor/outdoor storage if it is properly packaged.

  • The unit and accessories should be stored sealed with desiccants in aluminum foil and packed in a wooden box (the storing time before installation is complaint with the warranty period in the terms and conditions).

  • Pallets should not be removed until the installation.

  • The storage room environment should be healthy, no rodents, humidity control ≤ 95%/≤ 90% for 24 hours and one month respectively, and no water on the floor.

Store the device in their original packaging, placed on dry ground or on a material insulating it from environmental condition.

Storage Temperature

NOTICE
HAZARD OF EQUIPMENT CORROSION
Ensure that the equipment is not stored for longer than 6 months.
Failure to follow these instructions can result in equipment damage.

The unit storage conditions within the period are as follows:

  • Between 6 and 12 months, perform basic level preventive maintenance to help ensure the unit operates correctly.

  • Beyond 12 months, contact Schneider Electric Service local representative for check-up.

NOTE: The unit should be checked periodically for any signs of deterioration. It is recommended that unit must not be stored more than six months.

After unpacking, check the unit carefully for:

  • Absence of broken or damaged parts.

  • Absence of condensation marks or droplets.

  • Absence of visible degradation (color change, rust, deposits, and so on).

In case of any degradation detected, the unit should not be installed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?